PLC Variable Creation Wizard
This wizard allows you to automatically create a list of variables used for the mapping. The variable type is Boolean for digital I/Os and UINT for analog I/Os.
Figure 5-103: Wizard to Create PLC Variable - Parameters
| Field | Description |
|---|---|
| From channel | Defines the range of channels you want to map automatically |
| Scope | Defines where the variables are created (if you select the Global scope, then the variables are created under the Global node in the Dictionary) |
| Base Name | Pattern used for variable naming with the name of the object in the Project Tree, followed by a 2-letter acronym (2LA) representing the I/O type. The channel number will replace ##. |
Figure 5-104: Wizard to Create PLC Variable - Mapped Channels
Figure 5-105: Wizard to Create PLC Variable - Variables in the Dictionary
|
Copyright © 2018 Kollmorgen |
|