Forcing a variable

At run-timeClosedIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running, double-click on the value of the variable in the list or press the ENTER key when it is selected. A popup window appears and allows you to:


  • The value of a locked variable is displayed with square brackets.

  • Unlock: Remove the lock on a variable so it can be changed again by the runtime.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen