Display the IP Address of a PDMM or PCMM
The IP Address assigned to the controller can be shown on the 7-segment display. The IP may be displayed at boot and can be accessed from the PDMM or PCMM B3 Button Menu. Note that there is a 5 second delay before this function may be used again.
-
-
The AKD PDMM or PCMM will not set (or show) an IP address without an attached network cable.
|
Copyright © 2018 Kollmorgen |
|