Using the AKD PDMM or PCMM Controller

Tasks related to the controllers are:

  • Configure parameters
  • Start and stop your KAS application
  • Update the firmware
  • Reset to factory settings

Rebooting the controller, recovering the firmware, and resetting the controller may be performed from the device or, more conveniently, using the web server.


  • Please note that any reference to AKD PDMM or PCMM refers to both the 800MHz and the single- and dual-core 1.2GHz variants, unless otherwise noted.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen