Import a Control Panel
Control Panels may be exported and imported for easy reuse across projects. Any variables associated with the control panel will be preserved across projects.
- Right-click on Controller in the Project View and select Import Control Panel.
- Locate a saved .GRA file and click Open.
- If the panel you are trying to import has the same name as an existing panel, you will be prompted to change the name or cancel the import.
- If the panel you are trying to import has the same name as an existing panel, you will be prompted to change the name or cancel the import.
- Upon clicking Open (or OK) the panel will be placed in the Project View.
See also: Export a Control Panel
|
Copyright © 2018 Kollmorgen |
|