Channels Current channel Time base Time position 3 buttons

The Control Panel

As shown in Figure 7-24: Oscilloscope Control Panel, the control panel consists of the following items:

Scope Control Panel
  1. The Channels list
  2. The Current channel property
  3. The Time-base
  4. The Time position
  5. Five buttons

Figure 7-24: Oscilloscope Control Panel

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen