Mapping a Variable to the Oscilloscope

A probe (variable) can be directly plugged or mapped from within the Oscilloscope:

  1. Right-click on any channel (already mapped or not) in the channels list and select the Map option to open the Scope Variable Selector.

    • If your application is not connected and running, the following message is displayed.

  2. Navigate through the available variables and select the one you want to connect to the channel

    Variable Selector for Pipe Network

    Figure 7-32: Using the Variable Selector to choose a variable to be mapped in the Oscilloscope

  3. For more details on:

  4. (Optional) Set the Derivation Order.
  5. (Optional) Set the Derivation Period. The value entered should be either 0.0 (no modulo) or the Modulo Period, e.g. 360.0.
    If the selected Derivation Order is greater than zero, the Derivation Period of the selected signal can be used to remove rollover spikes in the derivative value if the variable is of a periodic nature as the result of "modulo" behavior.

You can also disconnect a probe as follows:

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen