Traces

The trace is the resulting graph of the variable's evolution against time, with the more distant past on the left and the more recent past on the right.


  • The acquisition of samples is limited to 100'000 cycles (ie. 100 s when cycle time is set to 1000 µs, and 25 s when cycle time is set to 250 µs). When you reach this limit:

    • The first data that are added to the queue are the first data to be removed (FIFO queue)
    • The start timing increases

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen