Help Menu

Command Description
Documentation Opens the help system.
Help Preference As stated in Is the Help System Online or Offline?, there is more than one type of help system with different advantages. By default the Online version is used. If you prefer, you may specify which Help version to use, the Online (default) or Offline (built-in) help system.
Kollmorgen Developer Network (KDN) Opens a web browser to the Kollmorgen Developer Network (www.kollmorgen.com/developer-network/), a community support site.
About Show version numbers and other information about the KAS IDEClosed"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger
Find KAS IDE Version

Table 5-7: Help Menu Commands

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen