ACTION#.CONDITIONVALUE
Description
ACTION#.CONDITIONVALUE defines the value used by ACTION#.CONDITION to test against the source. The range of this keyword depends on the value of ACTION#.SOURCE and ACTION#.CONDITION. Both must be set before setting the condition value. If ACTION#.CONDITION is modified, the range of the ACTION#.CONDITIONVALUE may change, and the value will return to default.
Some conditions do not require a condition value.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
Depends on ACTION#.SOURCE and ACTION#.CONDITION |
|
Default Value |
Depends on ACTION#.SOURCE and ACTION#.CONDITION |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
|
Copyright © 2018 Kollmorgen |
|