AIN#.DEADBANDMODE

Description

When AIN#.DEADBANDMODE is set to 0, and the value of the analog input is less than the absolute value of AIN#.DEADBAND, the analog command will be 0. When the analog input is greater or equal to the absolute value of AIN#.DEADBAND, then the analog command will be generated using the scaling specified.

When AIN#.DEADBANDMODE is set to 1, the analog command is 0 if the input is less than the absolute value of the deadband value. When the input is greater than the absolute value of the deadband, the output is equal to (Input - Deadband) * Scaling.

Below are illustrations of this behavior.

Examples

Context

For more information see Analog Input.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also  
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen