AOUT#.VALUE
Description
AOUT#.VALUE reads the analog output value.
Examples
Context
For more information see Analog Output.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read Only |
| Units | V |
| Range | 0 to 10V |
| Default Value | 0V |
| Data Type | Float |
| See Also | |
| Stored in Non Volatile Memory | No |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AOUT1.VALUE | 0x3800 | 0x1 | INT | 1000:1 | - | RO | True |
| AOUT2.VALUE | 0x3801 | 0x1 | INT | 1000:1 | - | RO | True |
|
Copyright © 2018 Kollmorgen |
|