AXIS#.GEAR.ACC

Description

AXIS#.GEAR.ACC defines the maximum acceleration limit that the axis will use to achieve the master position. As soon as the slave axis has achieved gearing lock with the master AXIS#.GEAR.ACC will no longer have an effect, and the slave will track the master regardless of the acceleration of the master.

Versions

Action Version Notes
Implemented 02-00-00-000
     

General Information

Type

Read/Write

Units

Rotary: RPMClosed"Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

See Acceleration Units for details.

Range

Depends on units. See Acceleration Range for details.

Default Value

10,000 RPM/s

Depends on units. See Acceleration Units for details.

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.GEAR.ACC 0x5006 0x1 UDINT - Acceleration RW False
AXIS2.GEAR.ACC 0x5106 0x1 UDINT - Acceleration RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen