AXIS#.HWEN.MODE

Description

Selects whether AXIS#.CLRFAULTS is performed on the rising edgeClosedA rising edge is the transition of a digital signal from low to high. It is also called positive edge of the hardware enable input

Examples

Usage

0 (default): perform AXIS#.CLRFAULTS on the rising edge of the hardware enable input

1: do not perform clear faults on the rising edge of the hardware enable input

Code

--> AXIS1.HWEN.MODE 0
--> AXIS2.HWEN.MODE 1

Context

For more information on hardware enable, refer to the Enable/Disable.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also AXIS#.HWEN.SOURCE, AXIS#.HWEN.STATE, AXIS#.CLRFAULTS

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.HWEN.MODE 0x5009 0x2 USINT - - RW False
AXIS2.HWEN.MODE 0x5109 0x2 USINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen