AXIS#.HWLS.NEGSTATE

Description

Returns the state of the negative hardware limit switch

Examples

Usage

0: negative limit switch is low

1: negative limit switch is high

Code

Axis 1 negative limit switch is low. Axis 2 negative limit switch is high.

-->AXIS1.HWLS.NEGSTATE
0
-->AXIS2.HWLS.NEGSTATE
1

Context

For more information on limit switches, refer to Limits.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units N/A
Range 0 to 1
Default Value N/A
Data Type Integer
See Also AXIS#.HWLS.NEGSOURCE
Stored in Non Volatile Memory No

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.HWLS.NEGSTATE 0x5015 0x1 USINT - - RO True
AXIS2.HWLS.NEGSTATE 0x5115 0x1 USINT - - RO True

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen