AXIS#.IL.FF

Description

AXIS#.ILClosed"Instruction list" This is a low-level language and resembles assembly.FF reads the present current loop overall feed-forwardClosedThis describes an element or pathway within a control system which passes a controlling signal from a source in the control system's external environment, often a command signal from an external operator, to a load elsewhere in its external environment value. It is the sum of the following feed-forward paths:

AXIS#.IL.FF is calculated using the following variables' values at the time it is called:

AXIS#.IL.FF = AXIS#.IL.KACCFF * Accelration Command + AXIS#.VL.KVFF * Velocity Command + AXIS#.IL.FRICTION (if motion is currently commanded) + AXIS#.IL.OFFSET (always) + * AXIS#.IL.BUSFF (if fieldbus connected)

For EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs:

AXIS#.IL.BUSFF is the injected current feedforward, which corresponds to Object 60B2h: Torque Offset. The scaling for the torqueClosedTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist offset is done with 1/1000 rated torque. In AKD, a value of 1000 means AXIS#.ICONT will be commanded in AXIS#.IL.BUSFF (if AXIS#.IL.KBUSFF is set to 1).

AXIS#.IL.KBUSSFF is a gain setting for the feedforward value AXIS#.IL.BUSFF. It needs to be set to greater zero to let AXIS#.IL.BUSFF take effect. AXIS#.IL.KBUSFF can be access by SDO object 50E2h/0.

The AXIS#.IL.BUSFF gain can be commanded through EtherCAT in all DS402 operating modes.

Versions

Action Version Notes
Implemented 02-00-00-000
     

General Information

Type

Read Only

Units

Arms

Range

N/A

Default Value

N/A

Data Type

Float

See Also

, AXIS#.IL.KVFF, AXIS#.IL.OFFSET, AXIS#.IL.FRICTION, AXIS#.IL.KACCFF

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Related Topics

Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen