AXIS#.IL.IFOLD
Description
Two current foldback algorithms run in parallel in the drive: the drive foldback algorithm and the motor foldback algorithm. Each algorithm uses different sets of parameters.
Each algorithm has its own foldback current limit, AXIS#.IL
"Instruction list"
This is a low-level language and resembles assembly.DIFOLD and AXIS#.IL.MIFOLD. The overall foldback current limit at any moment is:
AXIS#.IL.IFOLD = min (AXIS#.IL.DIFOLD, AXIS#.IL.MIFOLD, AXIS#.IPEAK)
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
General Information
|
Type |
Read Only |
|
Units |
A |
|
Range |
0 to 2,147,483.647 A |
|
Default Value |
N/A |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.IL.IFOLD | 0x500A | 0xC | DINT | 1000:1 | - | RO | False |
| AXIS2.IL.IFOLD | 0x510A | 0xC | DINT | 1000:1 | - | RO | False |
|
Copyright © 2018 Kollmorgen |
|