AXIS#.IL.VCMD

Description

Reads the output of the current loop that controls the q-component of the current.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

VrmsClosedrms stands for root mean square (also known as the quadratic mean) L-N

Range

0 Vrms to bus voltage

Default Value

N/A

Data Type

Float

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Related Topics

Current Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen