AXIS#.MOTOR.FIELDWEAKENING

Description

This parameter turns on field weakening control for rotary surface permanent magnet motors (AXIS#.MOTOR.TYPE = 0). Field weakening allows a motor to operate above rated speed, at constant power with reduced torqueClosedTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist.

This keyword can only be set when AXIS#.MOTOR.TYPE = 0. Any other AXIS#.MOTOR.TYPE will result in an error and AXIS#.MOTOR.FIELDWEAKENING will not be applied.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.MOTOR.FIELDWEAKENING 0x500B 0xF USINT - - RW False
AXIS2.MOTOR.FIELDWEAKENING 0x510B 0xF USINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen