AXIS#.MOTOR.LDLL

Description

This parameter is the motor line to line direct (flux producing) axis inductance.


  • This parameter is automatically configured for (Undefined variable: MyVariables.CompanyName) motors when AXIS#.MOTOR.AUTOSET = 1.


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 0, 1, 4, 6, and 8.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

mH

Range

1 to 2^31

Default Value

4

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen