AXIS#.MOTOR.NAME

Description

This parameter is the motor name.


  • This parameter is automatically configured for (Undefined variable: MyVariables.CompanyName) motors when MOTOR.AUTOSET=1.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

11 chars

Default Value

empty

Data Type

String

See Also

N/A

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen