AXIS#.MOTOR.PHASE

Description

This parameter is the relative alignment of the feedback to the motor coils. For (Undefined variable: MyVariables.CompanyName) motors, the feedback and coils are aligned, and AXIS#.MOTOR.PHASE may be set to 0.


  • If MOTOR.AUTOSET = 1 and motor memory version is 0.2 or greater, this parameter is automatically configured for Kollmorgen motors.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Electrical degrees

Range

0 to 360

Default Value

0

Data Type

Integer

See Also

N/A

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.MOTOR.PHASE 0x500B 0x15 UINT - - RW False
AXIS2.MOTOR.PHASE 0x510B 0x15 UINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen