AXIS#.MOTOR.TEMPFAULT

Description

This parameter is used to configure the motor temperature fault level as a resistance threshold of the motor thermal sensorClosedA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer.

A zero value prevents temperature faults from being reported.


  • This parameter is automatically configured for (Undefined variable: MyVariables.CompanyName) motors when AXIS#.MOTOR.AUTOSET = 1 and motor memory version is 0.3 or greater.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Ω

Range

0 to 2,000,000,000 Ω

Default Value

2000

Data Type

Integer

See Also

AXIS#.MOTOR.TEMP

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.MOTOR.TEMPFAULT 0x500B 0x1D UDINT - - RW False
AXIS2.MOTOR.TEMPFAULT 0x510B 0x1D UDINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen