AXIS#.MOTOR.VMAX
Description
This parameter is the maximum motor mechanical speed. The value 1.2 x AXIS#.MOTOR.VMAX becomes the overall overspeed fault threshold (AXIS#.VL.VFTHRESH) if it is less than the user overspeed fault threshold (AXIS#.VL.THRESH ), and for AXIS#.MOTOR.TYPE = 6 if it is less than the motor back EMF overspeed threshold ((1.02 x 1000 x VBUS.OVFTHRESH) / (AXIS#.MOTOR.KE x sqrt(2))).
-
-
This parameter is automatically configured for (Undefined variable: MyVariables.CompanyName) motors when AXIS#.MOTOR.AUTOSET = 1 and motor memory version is 0.2 or greater.
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
rpm |
|
Range |
100 to 40,000 rpm |
|
Default Value |
3,000 rpm |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.MOTOR.VMAX | 0x500B | 0x1F | UINT | - | - | RW | False |
| AXIS2.MOTOR.VMAX | 0x510B | 0x1F | UINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|