AXIS#.MOTOR.VOLTRATED

Description

This parameter configures the drive for the induction motor's rated voltage as indicated on the nameplate.

AXIS#.MOTOR.VOLTRATED is used to calculate the constant Volts per Hertz characteristics of the drive and motor.


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 2.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

V

Range

50 to 1,000 V

Default Value

230 V

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.MOTOR.VOLTRATED 0x500B 0x6 UINT - - RW False
AXIS2.MOTOR.VOLTRATED 0x510B 0x6 UINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen