AXIS#.MT.MOVE
Description
This command needs one argument in order to start a motion task. The drive must be homed, otherwise the motion task will not start.
Example
AXIS#.MT.MOVE 3 -> Start motion task number 3.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
General Information
This content is not applicable to KAS, using either a PAC
"Programmable Automation Controller"
PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system or a PDMM.
|
Type |
Command |
|
Units |
N/A |
|
Range |
0 to 31 |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Related Topics
0.1 Motion Tasks
|
Copyright © 2018 Kollmorgen |
|