AXIS#.MT.P
Description
Specifies the motion task position. Depending on the motion task control word (AXIS#.MT.CNTL), the AXIS#.MT.P command can either be the target position of the motion task or a relative distance.
Examples
Code
Sets the position of motion task 0 to 360 degrees. The first parameter is the motion task number and the second is the position.
-->AXIS1.MT.P 0 360
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS, using either a PAC
"Programmable Automation Controller"
PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system or a PDMM.
|
Type |
Read/Write |
|
Units |
Rotary: counts, rad, deg, custom units, 16-bit counts See Position Units for details. |
|
Range |
Depends on units. See Position Range for details. |
|
Default Value |
0 |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Related Topics
0.1 Motion Tasks
|
Copyright © 2018 Kollmorgen |
|