AXIS#.MT.TRANSITION
Description
This keyword sets the Motion Task ControlWord with the Motion Task Transition information.
It takes the following values:
| 0 | No Dwell |
| 1 | Dwell |
| 2 | Blend into acceleration (after MT end) |
| 3 | Blend into Velocity (before MT end) |
-
-
Transition Types 2 and 3 (Blending) may only be performed when both starting and following motion tasks are in the same direction. This motion type will turn two motion tasks into a continuous move that only comes to rest after the second move.
-
If Transition Type 2 or 3 is used on motion tasks which alternate direction, the motion tasks will still be performed but will be treated as a Dwell move with zero transition time in between motion tasks.
Examples
Usage
This keyword is used to set what you would otherwise have set with AXIS#.MT.CNTL.
Code
MT.TRANSITION 0 1 Will configure Motion Task 0 to dwell.
Context
See AXIS#.MT.CNTL for more information on the argument semantics.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 3 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | |
|
Stored in Non Volatile Memory |
No |
Variants Supported
Supported on all drives
|
Copyright © 2018 Kollmorgen |
|