AXIS#.UNIT.PROTARY

Description

AXIS#.UNIT.PROTARY sets the position units when the motor type (AXIS#.MOTOR.TYPE ) is rotary.

Value

Units

0

counts

1

rad

2

degs

3

Custom Units

4

counts 16-bit

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 4

Default Value

0

Data Type

Integer

See Also

AXIS#.PL.FB , AXIS#.PL.CMD , AXIS#.MOTOR.TYPE

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.UNIT.PROTARY 0x5010 0x5 USINT - - RW False
AXIS2.UNIT.PROTARY 0x5110 0x5 USINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen