AXIS#.VL.FBSOURCE

Description

This parameter determines the feedback source to be used by the velocity loop.

Value Definition
0 Defers selection to AXIS#.IL.FBSOURCE - this is the default, and uses the value which is being used for commutation
1 Selects FB1 (connector X1)
2 Selects FB2 (connector X2)
3 Selects FB3 (connector X23)
4 Selects FB4 (connector X21)
5 Selects FB5 (connector X22)

Versions

Action Version Notes
Implemented 02-00-00-000
     

General Information

Type

Read/Write

Units

N/A

Range

0 to 5

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Related Topics

Velocity Loop

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen