AXIS#.WS.CHECKT

Description

This parameter sets the amount of time a commutation error must be present before a fault occurs. Commutation monitoring is disabled when this parameter is set to 0.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

ms

Range

0 to 10,000

Default Value

10

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.WS.CHECKT 0x5013 0x10 UINT - - RW False
AXIS2.WS.CHECKT 0x5113 0x10 UINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen