AXIS#.WS.CHECKV
Description
This parameter sets the velocity threshold which has to be exceeded to activate commutation monitoring.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
||
|
Units |
Rotary: RPM See Velocity Units for details. |
||
|
Range |
Depends on units. See Velocity Range for details. |
||
|
Default Value |
N/A |
||
|
Data Type |
Float |
||
|
Stored in Non Volatile Memory |
Yes |
||
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.WS.CHECKV | 0x5013 | 0xB | DINT | - | Velocity | RW | False |
| AXIS2.WS.CHECKV | 0x5113 | 0xB | DINT | - | Velocity | RW | False |
|
Copyright © 2018 Kollmorgen |
|