AXIS#.WS.TIRAMP
Description
In Wake & Shake mode 1, a maximum current of AXIS#.WS.IMAX is applied to the AXIS#.MOTOR. AXIS#.WS.TIRAMP defines a time to reach this maximum current. Longer times are useful for big inertia motors or heavy loads.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
ms |
|
Range |
512 to 10,000 |
|
Default Value |
512 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.WS.TIRAMP | 0x5013 | 0x11 | UINT | - | - | RW | False |
| AXIS2.WS.TIRAMP | 0x5113 | 0x11 | UINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|