AXIS#.EN

Description

AXIS#.EN issues a software enable to the axis. Check AXIS#.ACTIVE to determine if the axis is enabled or disabled.

You can also query the value of AXIS#.DISSOURCES to check whether the software enable bit is high (software enabled was issued by executing AXIS#.EN) or the software enable bit is low (software disable was issued by executing AXIS#.DIS). If the axis software enable bit is low and AXIS#.EN is executed, then axis faults are automatically cleared during the software enable process.

Example

Code

Enables Axis 1:

-->AXIS1.EN

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

AXIS#.DIS | AXIS#.DISSOURCES ,AXIS#.ACTIVE

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Related Topics

Enable/Disable

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen