BRAKE#.AXIS

Description

Sets which axis will control the brake.

Value Description
0 Not used
1 Controlled by Axis 1.
2 Controlled by Axis 2.

Examples

Context

For more information see Brake.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 2

Default Value

Depends on Brake and Axis number:

BRAKE1 defaults to 1.

BRAKE2 defaults to 2 on multi-axis drives and 0 on single-axis drives.

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen