DIN#.STATE

Description

Reads the state of one digital input according to the number identified in the command.

Examples

Code

--> DIN1.STATE
1

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units N/A
Range 0 to 1
Default Value N/A
Data Type Integer
See Also  

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen
Index 0x60FD
Subindex 0x0
Data Type UDINT
Float Scale N/A
Access Read Only
PDO Map TX Pdo

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen