DIO#.STATE

Description

Reads the state of the specified bi-directional channel.

Examples

Code

--> DIO1.STATE
1

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units N/A
Range 0 to 1
Default Value N/A
Data Type Integer
See Also  

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen