DOUT#.SOURCEID
Description
Gets or sets the digital output source id. Value sets the compare engine being used when DOUT#.SOURCE = 3 (Compare)
Examples
Usage
When DOUT#.SOURCE = 3 (Compare) and DOUT#.SOURCEID = 1. DOUT#.STATE will be the result of compare engine 1.
Context
For more information see Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | N/A |
| Default Value | 0 |
| Data Type | Integer |
| See Also | |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
0x360A | DOUT1.SOURCE | 0x1 | USINT | - | - | RW | False |
| DOUT2.SOURCE | 0x1 | USINT | - | - | RW | False | ||
| DOUT3.SOURCE | 0x1 | USINT | - | - | RW | False | ||
| DOUT4.SOURCE | 0x1 | USINT | - | - | RW | False | ||
| DOUT5.SOURCE | 0x1 | USINT | - | - | RW | False | ||
| DOUT6.SOURCE | 0x1 | USINT | - | - | RW | False | ||
| DOUT7.SOURCE | 0x1 | USINT | - | - | RW | False | ||
| DOUT8.SOURCE | 0x1 | USINT | - | - | RW | False | ||
| DOUT9.SOURCE | 0x1 | USINT | - | - | RW | False |
|
Copyright © 2018 Kollmorgen |
|