DRV.DOWNLOADALLOWED

Description

This parameter returns whether the drive is in a safe state to begin a firmware download. A download can only be performed if the value is one. If the value is zero, WorkBench will block the download.

For an AKD2G or NSD, the value depends on the drive enable status. For a CPS, the value depends on the enable states of the NSDs on its string. If one more more NSDs are enabled on a string, download to the CPS will be blocked.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

0 to 1

Default Value

N/A

Data Type

Integer

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Related Topics

Limits

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen