EEO#.MODE
Description
This keyword specifies the type of output waveform an EEO generator will create.
| SOURCE | ||
|---|---|---|
| 0 (default) | A Quad B |
|
| 1 | CW/CCW |
|
| 2 | Step/Direction |
|
Examples
Code
This will set the 2nd EEO output mode to Clockwise/Counter-clockwise.
-->EEO2.MODE 1
Context
For more information see Encoder Emulation.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 2 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.
|
Copyright © 2018 Kollmorgen |
|