Form Fill and Seal Pipe Network

Introduction

This application module details a 5 axis form, fill, and seal machine (FFS) using the Pipe Network motion engine. The unwind axis maintains a desired tension on the film as the film transport; using registration marks on the film; positions the film. When in position the filling screw fills the bag, the sealing jaw will seal the bag, and the flying shear will cut on the seal to provide each individually formed, filled, and sealed bag.

  1. Filling Screw (via cam)
  2. Film transport unit to RM
  3. Unwinding
  4. Sealing jaw
  5. Flying Shear

Figure 8-218: Form Fill and Seal Machine Overview

Pipe Network

The combination of pipeblocks and PLCClosed"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events code can easily be modified for use in a variety of form fill and seal applications, by modifying the CAM profiles and machine cycle times to fit machines with varying mechanics and desired material cut lengths.

Unwind Axis

The unwind axis is geared to the virtual master axis. As the film is being unwound from the parent roll a dancer roll is monitoring the desired tension. If the tension is outside the desired adjustable dead band the gear ratio between the virtual master axis and unwind is adjusted to maintain the desired tension. The tension (Regulation Tn), gain to control the tension (Regulation Kp), minimum and maximum dead band (Min Deadband & max Deadband) is entered on the control panel.

Filling Axis

The filling axis is geared to the master virtual axis based on a profile (FillingPro). The phase shift, speed, and quantity variables for the filling screw are entered on the operator panel. The phase shift is the position on the master axis that the filling axis profile (FillingPro) will start. The speed is the time from the start position to a point in the master position that the filling screw profile follows the master. The quantity is the amount of the “FillingPro” profile to be executed.

Figure 8-219: Filling Screw Base Profile

Film Transport Axis

The film transport axis monitors the registration marks on the film and adjusts the film based on the registration mark parameters, Open Window, Close Window, and Reference Pos entered on the operator panel. If the registration mark is detected between the Open Window and Close Window the registration mark is considered a good mark and the Reference Pos value will be used to calculate the necessary adjustment. If the registration mark is detected outside the Open Window and Close Window values then the registration mark is ignored. Adjustments are not made during the seal process to avoid destroying product.

Sealing Jaw

The sealing jaw axis is geared to the master virtual axis based on two profiles (SealBarClose and SealBaropen). The profile will start at the same starting position as the flying shear. The sealing time is entered at the operator interface.

Figure 8-220: Sealing Jaw Base Profile

Flying Shear

The flying shear axis is geared to the master virtual axis based on a profile (FlySaw). The profile will start at the phaseshift entered at the operator interface.

Figure 8-221: Flying Shear Base Profile

PLC Program Code

Key FunctionClosedA function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. Blocks and Kollmorgen UDFBs used in the application

Name How Used

MC_GearIn

Gears one axis to another

MC_CamIn

Gears one axis to another using a cam profile

MC_TouchProbe

Arms the fast inputClosedThe inputs are taken into account at each cycle depending on the system periodicity (for example each millisecond). Under certain circumstances this can be insufficient when more accuracy is needed, or if a quick response is required from the system. To fill the gap, a drive may have some Fast Input connections (generally one or two). When an event happens that triggers a Fast Input (e.g. when a sensor sends a rising edge), the detection of a signal occurs faster (which can be 1000 times more accurate than the system periodicity). Then the timestamp associated with this input can be provided to the IPC to take corrective action and returns the latched position when the fast input occurs

The main section of the PLC code contains several If/Then statements. The program sets up gearing and cam profiles for the slave axis to a virtual master. The virtual master controls the machine speed. The slave axes are manipulated by either changing the operator panel inputs or profiles. The program is monitoring registration marks on the film and making correction to the film position based on the entries at the operator panel.

 

//****************

// Machine Control

//****************

IF bStart THEN

fStart(bStart);

IF OldMachineSpeed<>MachineSpeed THEN

      MLMstRun(PipeNetwork.MASTER, MachineSpeed);

      OldMachineSpeed:=MachineSpeed;

END_IF;

ELSE

IF fStart.Q THEN

      MLMstWriteSpeed(PipeNetwork.MASTER, MachineSpeed);  

      MLMstAbs(PipeNetwork.MASTER, 720.0);

      OldMachineSpeed:=0.0;

END_IF;

END_IF;

 

 

//***************

// Dancer Control

//***************

// Range 0-10V, 5V mid, 4-6V Deadband, <4V increase speed, >6V decrease speed

IF bStart THEN

IF (AnaInDancer<MinDeadBand) THEN

      DancerGear:=(AnaInDancer-DancerRef)*Kp;

IF Tn>0.0 THEN

         DancerGearI:=OldDancerGearI+(AnaInDancer-DancerRef)*Kp/Tn*1000;

         OldDancerGearI := DancerGearI;

ELSE

         DancerGearI := 0.0;

         OldDancerGearI := 0.0;

END_IF;

      DancerGear := DancerGear+DancerGearI;

IF DancerGear > LREAL#1.0 THEN

         DancerGear:=LREAL#1.0;

         OldDancerGearI := LREAL#1.0;

ELSIF DancerGear < LREAL#-1.0 THEN

         DancerGear:=LREAL#-1.0;

         OldDancerGearI := LREAL#-1.0;

END_IF;

      OldDancerGear:=DancerGear;

      MLGearWriteRatio(PipeNetwork.DancerCtrl, (LREAL#1.0+DancerGear));

ELSIF (AnaInDancer>MaxDeadBand) THEN

      DancerGear:=(AnaInDancer-DancerRef)*Kp;

IF Tn>0.0 THEN

         DancerGearI:=OldDancerGearI+(AnaInDancer-DancerRef)*Kp/Tn*1000;

         OldDancerGearI := DancerGearI;

ELSE

         DancerGearI := 0.0;

         OldDancerGearI := 0.0;

END_IF;

      DancerGear := DancerGear+DancerGearI;

IF DancerGear > LREAL#1.0 THEN

         DancerGear:=LREAL#1.0;

         OldDancerGearI := 1.0;

ELSIF DancerGear < LREAL#-1.0 THEN

         DancerGear:=LREAL#-1.0;

         OldDancerGearI := LREAL#-1.0;

END_IF;

      OldDancerGear:=DancerGear;

      MLGearWriteRatio(PipeNetwork.DancerCtrl, (LREAL#1.0+DancerGear));

ELSE

// Deadband

END_IF;

 

END_IF;

 

 

//*************

// Filling axis

//*************

IF MLCompCheck(PipeNetwork.AdjustFilling) THEN

   MLCompReset(PipeNetwork.AdjustFilling);

MLPhaWritePhase(PipeNetwork.StartFilling,PhaseFilling);

   MLPrfWriteIScale(Profiles.FillingPro,IRatioFilling);

   MLPrfWriteOScale(Profiles.FillingPro,ORatioFilling);

END_IF;

 

 

//*****************************************

// Transport axis with registration control

//*****************************************

IF MLCompCheck(PipeNetwork.WindowCtrl) THEN

IF bWindowOpen THEN

      MLCompWriteRef(PipeNetwork.WindowCtrl, (OpenWindow<MLBlkReadOutVal(PipeNetwork.WindowCtrl)), OpenWindow);

      MLCompReset(PipeNetwork.WindowCtrl);

      bWindowOpen:=FALSE;

IF MLTrigIsTrigged(PipeNetwork.RegMark) THEN

         CorrLength:=MLTrigReadPos(PipeNetwork.RegMark)-ReferencePos;

IF CorrLength>MaxCorrLength THEN

            CorrLength:=MaxCorrLength;

ELSIF CorrLength< -MaxCorrLength THEN

            CorrLength:=-MaxCorrLength;

END_IF;

ELSE

         CorrLength:=MaxCorrLength;

END_IF;

      MLPhaWritePhase(PipeNetwork.PHCorr,LREAL#-1.0*CloseWindow);

      MLPrfWriteOScale(Profiles.Corr, CorrLength);

ELSE

      MLCompWriteRef(PipeNetwork.WindowCtrl, (CloseWindow<MLBlkReadOutVal(PipeNetwork.WindowCtrl)), CloseWindow);

      MLCompReset(PipeNetwork.WindowCtrl);

      bWindowOpen:=TRUE;

      MLTrigClearFlag(PipeNetwork.RegMark);

      MLAxisRstFastIn(PipeNetwork.Transport, 0);

END_IF;

END_IF;

    

 

//**********

// Flying saw

//**********

IF PhaseFlySaw <> OldPhaseFlySaw THEN

   MLPhaWritePhase(PipeNetwork.PHFlSaw,PhaseFlySaw);

   OldPhaseFlySaw := PhaseFlySaw;

END_IF;

  

 

//************

// Sealing bar

//************

IF MLCompCheck(PipeNetwork.SealTimeCtrl) THEN

   MLCompReset(PipeNetwork.SealTimeCtrl);

   MLPhaWritePhase(PipeNetwork.PHSealBarOpen,LREAL#-270.0);

IF bStart THEN

      bStartSealTimer := TRUE;

END_IF;

END_IF;

 

TimerSealing(bStartSealTimer,SealTime);

IF TimerSealing.Q THEN

   bStartSealTimer := FALSE;

   MLPhaWritePhase(PipeNetwork.PHSealBarOpen,LREAL#-1.0*MLBlkReadOutVal(PipeNetwork.SealTimeCtrl));

   MLPrfWriteOScale(Profiles.SealBarOpen,360.0);

   MLPrfWriteOOffset(Profiles.SealBarOpen,LREAL#-90.0);

END_IF;

 

 

//******************

// Reset axis errors

//******************

IF bReset THEN

   MLAxisClrErrors(PipeNetwork.Unwind);

   MLAxisClrErrors(PipeNetwork.Filler);

   MLAxisClrErrors(PipeNetwork.Transport);

   MLAxisClrErrors(PipeNetwork.FlyingSaw);

   MLAxisClrErrors(PipeNetwork.SealingBar);

   bReset := FALSE;

END_IF;

Operator Panel

The Kollmorgen Automation Suite (KAS) program for this application module has an internal operator panel. The operator panel is used to set the desired values for each product and to start and stop the machine. The specific entries are described in the axis sections above. Below is a screen print of the operator panel.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen