AIN.OFFSET
Description
AIN.OFFSET sets the analog offset, which is added to the analog input command to the drive. This value compensates for the analog input signal (AIN.VALUE ) offset or drift.
General Information
|
Type |
NV Parameter |
|
Units |
V |
|
Range |
–10 to +10 V |
|
Default Value |
0 V |
|
Data Type |
Float |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
Variants Supported
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5003h/0 |
M_01-00-00-000 |
Related Topics
Analog Input (pg 1)
Block Diagram for Position/Velocity Loop
|
Copyright © 2018 Kollmorgen |
|