AOUT.DEBUGDATATYPE

Description

AOUT.DEBUGDATATYPE is used in AOUT.MODE = 9 (debug mode).

This parameter sets the data type of the value to be debugged according to the table below:

Value Data Type

0

Illegal type

1

Signed (1 byte)

2

Unsigned (1 byte)

3

Signed (2 bytes)

4

Unsigned (2 bytes)

5

Signed (4 bytes)

6

Unsigned (4 bytes)

7

Signed (8 bytes)

8

Unsigned (8 bytes)

9

Pointer to one byte

10

Fix shift

General Information

Type

NV Parameter

Units

N/A

Range

0 to 10

Default Value

0

Data Type

Integer

Start Version

M_01-01-01-000

Related Topics

Analog Output

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen