AOUT.ISCALE
Description
AOUT.ISCALE sets the analog current scale factor that scales the analog output (AOUT.VALUE) for AOUT.MODE = 4 or 5. The value entered is the motor current per 10 V of analog input or output. This value may be either higher or lower than 100%, but the actual analog I/O will be limited by the application current limit (IL.LIMITN and IL.LIMITP ).
General Information
|
Type |
NV Parameter |
|
Units |
A/V |
|
Range |
0.001 to 22.4 A/V |
|
Default Value |
0.001 to 22.4 A/V |
|
Data Type |
Float |
|
Start Version |
M_01-01-01-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5009h/0 |
M_01-00-00-000 |
Related Topics
|
Copyright © 2018 Kollmorgen |
|