Description
This parameter sets the analog output offset.
General Information
Type
NV Parameter
Units
V
Range
-10 to +10 V
Default Value
0 V
Data Type
Float
Start Version
M_01-00-00-000
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design
Index/Subindex
Object Start Version
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen
500Bh/0
Related Topics
Analog Output
Stay Connected with Kollmorgen
Copyright © 2018 Kollmorgen