BODE.EXCITEGAP
Description
BODE.EXCITEGAP controls how often the excitation is updated. The excitation is updated every n drive samples, where n is BODE.EXCITEGAP. For example, if BODE.EXCITEGAP = 2, then the excitation is updated every 2/(16,000 Hz) = 1/8,000 Hz = 0.000125 sec. When measuring a system, update the excitation only as often as the data is recorded.
Example
Set excitation update rate to 8,000 Hz:
-->BODE.EXCITEGAP 2
Set excitation update rate to 4,000 Hz:
-->BODE.EXCITEGAP 4
Get excitation update rate (already set to 8000 Hz):
-->BODE.EXCITEGAP 2
General Information
|
Type |
R/W Parameter |
|
Units |
Drive samples |
|
Range |
1 to 255 drive samples |
|
Default Value |
2 drive samples |
|
Data Type |
N/A |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5013h/0 |
M_01-00-00-000 |
Related Topics
Using the Performance Servo Tuner | Using the Performance Servo Tuner: Advanced
|
Copyright © 2018 Kollmorgen |
|