BODE.VFTHRESH
Description
When BODE.MODE is set to 5, the firmware monitors the drive feedback velocity VL.FB. When VL.FB goes above BODE.VFTHRESH, an internal counter records the length of time VL.FB was above BODE.VFTHRESH. If the internal counter reaches BODE.VFLIMIT, Fault 133 – Instability during Autotune will be generated.
The smaller BODE.VFLIMIT, the quicker Fault 133 will be generated when VL.FB exceeds BODE.VFLIMIT.
Example
Set BODE.VFTHRESH to 10 RPM
"Revolutions per minute"
Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component:
-->BODE.VFTHRESH 10
Set BODE.VFLIMIT to 0.500 seconds:
-->BODE.VFLIMIT 0.5
Set BODE.MODE to 5 to enable stability detection:
-->BODE.MODE 5
General Information
|
Type |
R/W Parameter |
|
Units |
Rotary: rpm, rps, deg/s, rad/s Linear: counts/s, mm/s, µm/s |
|
Range |
Rotary: 0.000 to 15,000.000 rpm 0.000 to 250.000 rps 0.000 to 90,000.000 deg/s 0.000 to 1,570.796 rad/s Linear: 0.000 to 1,073,741,824,000.000 counts/s 0.000 to 8,000.000 mm/s 0.000 to 8,000,000.000 µm/s |
|
Default Value |
0 |
|
Data Type |
Decimal |
|
Start Version |
M_01-02-10-000 |
Variants Supported
Related Topics
Using the Performance Servo Tuner
Using the Performance Servo Tuner: Advanced
BODE.MODE, BODE.MODETIMER, BODE.IFLIMIT, BODE.IFTHRESH, BODE.VFLIMIT
|
Copyright © 2018 Kollmorgen |
|