CMPx.WIDTHTYPE
Description
Use this keyword to set the width-type for a Compare setpoint
Setpoint is the target value that an automatic control system, for example PID controller, will aim to reach. The width-type determines whether the width of the Compare pulse is in position counts or units of time (microseconds).
Example
The following example sets the width type of setpoint 7 to microseconds, and the width of setpoint 7 to 1000 microseconds.
-->CMP0.WIDTHTYPE 7 1
-->CMP0.WIDTH 7 1000
General Information
|
Type |
NV Parameter |
|
Units |
None |
|
Range |
Argument 1: 0 to 7 Argument 2: 0 (position) to 1 (time) |
|
Default Value |
0 |
|
Data Type |
Argument 1:Integer Argument 2: Integer |
|
Start Version |
M_01-13-00-000 |
Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.
| AKD Type | Hardware Revision Supported |
|---|---|
| AKD | Revision D or higher |
| AKD PDMM | Revision DB or higher |
| AKD-T-IC |
Revision DA or higher |
| Fieldbus |
Index/Subindex | Object Start Version | |
|---|---|---|---|
| 34ACh/1 | CMP0.WIDTHTYPE 0 | M_01-13-00-000 | |
| 34AAh/2 | CMP0.WIDTHTYPE 1 | ||
| 34AAh/3 | CMP0.WIDTHTYPE 2 | ||
| 34AAh/4 | CMP0.WIDTHTYPE 3 | ||
| 34AAh/5 | CMP0.WIDTHTYPE 4 | ||
| 34AAh/6 | CMP0.WIDTHTYPE 5 | ||
| 34AAh/7 | CMP0.WIDTHTYPE 6 | ||
| 34AAh/8 | CMP0.WIDTHTYPE 7 | ||
|
34BCh/1 |
CMP1.WIDTHTYPE 0 | ||
|
34BAh/2 |
CMP1.WIDTHTYPE 1 | ||
|
34BAh/3 |
CMP1.WIDTHTYPE 2 | ||
|
34BAh/4 |
CMP1.WIDTHTYPE 3 | ||
|
34BAh/5 |
CMP1.WIDTHTYPE 4 | ||
|
34BAh/6 |
CMP1.WIDTHTYPE 5 | ||
|
34BAh/7 |
CMP1.WIDTHTYPE 6 | ||
|
34BAh/8 |
CMP1.WIDTHTYPE 7 | ||
Related Topics
|
Copyright © 2018 Kollmorgen |
|