COGCOMP.CORRECTIONTABLE

Description

Reads or writes to the cogging compensation table.

Examples

Reads the full table:

COGCOMP.CORRECTIONTABLE

Reads the compensation value for index "x":

COGCOMP.CORRECTIONTABLE x

Writes the value "y" to the table at index "x":

COGCOMP.CORRECTIONTABLE x y

General Information

This content is not applicable to KAS, using either a PACClosed"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system or a PDMM.

Type

R/W Parameter

Units

mA

Range

Argument 1: 0 to 8,191

Argument 2: 1.628 * DRV.IPEAK

Default Value

0

Data Type

Integer

Start Version

M_01-14-06-001

Related Topics

 

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen