CS.TO
Description
CS.TO is the time value for the drive velocity to be within CS.VTHRESH before the drive disables.
Example
Set time value to 100 ms:
-->CS.TO 100
General Information
|
Type |
NV Parameter |
|
Units |
ms |
|
Range |
1 to 30,000 ms |
|
Default Value |
6 ms |
|
Data Type |
Integer |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
3440h/3 |
M_01-00-00-000 |
Related Topics
CS.DEC , CS.VTHRESH , CS.STATE, DRV.DIS, DIN1.MODE TO DIN7.MODE, DRV.DISMODE, DRV.DISSOURCES
|
Copyright © 2018 Kollmorgen |
|